Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 15

This slide shows the ST process discussed in the previous slides, starting with the core, the brain of the meters which is the microcontroller. ST is a leader in the field in ARM Cortex-M microcontrollers. As can be seen, starting on the left with the STM8, the 8-bit microcontroller family with an ST proprietary core, and progressing to full ARM implementation using the Cortex-M3 lower power L1 to the F1 at 72 MHz in the DSP optimized Cortex-M4 core, to the F3, and finally leading to the STM32F4. The applications extend from low end meters to complicated ones, and to concentrators. Additional information is available on the STMicroelectronics website, www.st.com, including a dedicated presentation on microcontrollers.

PTM פורסם ב: