Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 25

In order to have forty million meters installed in the world during the last five years, it is necessary to be part of several alliances, to be part of standards definition; not only to be active members, but also part of the definition of the standard itself. Shown on this slide is a review of which standards ST is a part of and which standards their devices apply to. From the very beginning, ST worked with the Prime Alliance which offers embedded 130 kbps narrow band meter with OFDM capability as well as Meters and More, OPENMeter, and Open Standard that are working with lower speeds. ST is also strongly connected with the Home Plug Powerline Alliance, which applies the broadband power line technology. This is not used very much in the Smart Meter application; mostly in the smart goods utilization networks inside the house. ST works with standards from Spain, Italy, the U.S., and China; nearly all of the standards throughout the world. Latin America has not yet defined their own standards, but they are currently re-using some of the European standards.

PTM פורסם ב: