Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 41

A poly-phase meter implementation, as previously mentioned, does not use the standard meter chip, but the STPMC1 or S1 or S2. With the poly-phase meter implementation, the reference design embeds the anti-tampering function with ST’s MEMS. IrDA transmission with USB connectivity is being used as well, with fully embedded power management from ST. In this case, the power line is being used for communication. The STEVAL-IPP001V2 is a more complex board with more features, higher sensitivity, and embedded FreeRTOS firmware that can be modified for the customer’s use. A special card is used to support the Smartcard interface, with a ZigBee connector and the dual EEPROM as well. This modular solution is a complete meter with ST capability embedded.

PTM פורסם ב: