Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 27

The STarGRID platform represents the first approach to an SOC by embedding a front end, a dual core machine that runs both physical layer, a MAC layer, and a portion of the network layer with all the power requirements inside. ST has a communication node embedded in a chip with a high level of flexibility and programmability for either open standard or fully customized implementations. With the STarGRID, the user can communicate long distance with the powerful power amplifier that outputs up to 1 A output. Plus the STarGRID is pin-to-pin compatible from standard 2.4 kbps S-FSK up to 130 kbps OFDM, therefore the user can decide to go from one data rate to another data rate and have the same footprint on the communication devices resulting in a powerful machine. Protocol is typically embedded because ST is compliant with several standards. There is also a possibility for the user to run their own protocol on the ST7580, for example, where access is allowed to the MAC layer and the network layer.

PTM פורסם ב: