Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
MOSFETs-Slide3

A MOSFET works when a voltage is applied between the gate and the source. The MOSFET will turn on, and will allow current to flow from the drain to the source. A MOSFET typically, can be used as a signal amplifier similar to a power transistor. This is what is called linear operation of the device. However, the most common use of the MOSFET is the commutation between conduction and interdiction states, as a solid state switch. In most of the applications, this device is able to perform thousands of commutations per second.

PTM פורסם ב: