Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
STM660x Smart On-Off Controller Slide 20

There are also three additional functions provided by the STM660x: A Vref pin that provides a 1.5V reference voltage that is 1% accurate, a PB out pin that allows for the monitoring of the state of the pushbuttons, and a VCClo pin to monitor the Vcc voltage, preventing the battery from over-discharging.

PTM פורסם ב: