Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
EMC-Slide8

The impedance of a chip bead is composed of a frequency dependent resistance and a parallel inductance. From equation (1), the resistance of chip bead depends on the relative permeability (µs) of the ferrite materials with frequency characteristics as determined by the permeability value. The chip bead reduces the high frequency noise by using the resistance (loss) component of the impedance. The frequency where the resistive value becomes higher than the inductive value is known as the cross-point. The bead usage and value should be determined with this cross-point in mind.

PTM פורסם ב: