Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Modular Jack Portfolio Slide 21

The multi-port or ganged modular jacks will save space and room on customers’ PCB. Instead of using two single port connectors for example, the customer can choose to use a 1 x 2 multi-port configuration. Multi-port configurations are also available with a mix of jack type – for example there are connectors available that feature one RJ11 port and one RJ45 port in one 1 x 2 multi-port configuration. This provides additional flexibility to those customer applications that require two types of modular jacks in the same space.

PTM פורסם ב: