Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
ESD/EMI Protection Slide 13

Key considerations for ESD clamps are listed in this slide, plus graphs illustrating the two types of breakdown voltage. The first of these is the normal zener diode I-V relationship. Breakdown voltage is highlighted at the current ramp. The second is specific to TI components, illustrated by the I-V curve of a Snap Back which breaks down at Vbr, and then snaps back to Vsb. Side-by-Side Comparison of the two graphs makes it possible to visually see why Snap Back is a better solution than the normal Zeners.

PTM פורסם ב: