Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
USB-to-Serial Bridge Implementation Using the TUSB3410 Slide 7

The latest version of TUSBWINVCP is a single driver installer as opposed to the older version that was a two-part driver installation. In the older versions, the first part is for the USB “half” of the device, while the second part is for the virtual COM port. With the new single driver installation, it will only show up in the device manager as a COM PORT – in this example COM3.

PTM פורסם ב: