Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Battery-Mgmt-Pt2-Slide14

Here is an illustration of the error between the actual capacity of a Li-Ion and the capacity reported by the fuel gauge. This shows three curves corresponding to reported error at 3%, 5%, and 10% state of charge for a battery that was charged and discharge cycled 250 times. In all cases, the reported error was less than 1% from the actual capacity of the battery over 250 cycles.

PTM פורסם ב: