Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Code Composer Support for the Concerto Line Slide 10

After both cores are connected, the debug window looks much the same as it does with every other C2000 device, even though there are two cores. In order to control each of the cores independently, begin by selecting which core to take action with on in the debug window. In the example shown the C28 core has been selected, by clicking the run or stop or single step button, that action in the CCS will be on the control subsystem of the device.

PTM פורסם ב: