Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
eZ430 Chronos Development Tool Slide 5

The eZ430-Chronos provides nearly infinite possibilities by communicating with a broad range of devices. By simply adding a compatible wireless transceiver to an existing device, the user will now be able to control it or get information about it directly from the wrist. For example, information could be retrieved from the home thermostat as well as the temperature could be changed from anywhere in the home. Also, a computer can be paired to run a home media server so the Chronos could be used as a remote control. The buttons on the watch or the motion of the wrist can be used to control just about anything the user interacts with.

PTM פורסם ב: