Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Machine Interface Encoders

Take a look at this video shown here of a treadmill application. It’s speed range is 42 RPM to 3300 RPM, and the load can vary significantly from less than 100 lbs. to several hundred lbs. This machine was well-tuned for higher speed and load ranges, but the designers were having trouble controlling the system at low speed.

PTM פורסם ב: