Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
What is Bluetooth Slide 17

Lastly, this presentation will look at how Bluetooth® compares to other wireless technologies. In the first graph on the slide, the range of each technology is represented. As has been mentioned previously, Bluetooth has a typical range of 10 m, along with ANT and BLE. When considering data rate, or maximum throughput, Bluetooth ranks second to WiFi with a throughput of 2.1 Mpbs. ANT and BLE enable Bluetooth functionality in lower power applications, powered by coin cells and show slightly lower throughput at 1 Mbps. Bluetooth requires a AAA battery power source. In the graphs shown, it can be seen how other wireless technologies compare to Bluetooth from range, throughput and power perspectives.

PTM פורסם ב: