Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Introduction to the CC26xx Bluetooth LE Slide 11

How can developers get started with all this hardware and software?  There are two major choices depending where the customer is in development. If they want to quickly prototype how Bluetooth SMART would work in an application, then the SimpleLink SensorTag is the best place to start. If they are ready for product development with an easier debugging environment, users can use the development kit shown on the right which includes two LCD-enabled base boards and two RF-optimized EM boards. The CC2650DK also comes with a Bluetooth Smart USB stick to leverage TI’s PC-based tools.

PTM פורסם ב: