Maker.io main logo

32x32 Square Pixel Art Animation Display

456

2021-06-29 | By Adafruit Industries

License: See Original Project 3D Printing Adafruit Feather

Courtesy of Adafruit

By Ruiz Brothers

Overview

 

 

 

Retro Pixel Display

This is a square pixel display that uses an 32x32 RGB matrix display. It's powered by the Feather RP2040 and RGB Matrix FeatherWing. This runs CircuitPython and the Matrix Portal Library to play animated sprite sheets on the display.

display_1

RP2040 & RGB Matrices

The Feather RP2040 and RGB Matrix FeatherWing are mounted to a 3D printed frame on the back of the display. Paired with the FeatherWing Doubler, it’s easy to swap out the Feathers for future projects.

matrices_2

Black LED Acrylic

A sheet of black LED acrylic fits over the display and diffuses the LEDs. The 3D printed grid fits over the PCB with each LED enclosed in a square. This separates each LED and blocks the light from leaking into each square.

LED_3

Prerequisite Guides

Take a moment to walk through the following guides:

Parts from Adafruit

List of parts required for this build.

  • 32x32 RGB Matrix - 6mm Pitch

  • Feather RP2040

  • FeatherWing Doubler

  • RGB Matrix (M4+M0+RP2040) FeatherWing

  • Black LED Acrylic 12x12in

  • 5V 10A Power Supply

  • M2.5 Hardware Kit

Parts_4

CAD Files

CAD Files

STL files for 3D printing are oriented to print "as-is" on FDM style machines. Parts are designed to 3D print without any support material. Original design source may be downloaded using the links below.

  • frame.stl

  • grid.stl

  • cover.stl

  • feet.stl

CAD_5

Parts require minimum build volume: 210mm x 210mm

CAD Assembly

The black LED acrylic is fitted into the cover. The 32x32 RGB Matrix PCB is placed inside the frame with the grid fitted on top. The frame and grid are press fitted into the cover.

The Doubler FeatherWing is secured to the frame using M2.5 hardware standoffs and screws.

Feet are optionally secured to the bottom of the frame using M3 hexnuts and screws.

assembly_6

Grab just the STL files for 3D printing.

Download STL Files

Includes a STEP and Fusion 360 Archive.

Download CAD Source

Opens in the web browser to preview 3D models. More download options available in the preview page.

Fusion 360 Share Link

Acrylic PDF Template

Print the template on a sheet of paper. Ensure the scale is 100% when printing to get the correct dimension.

template_7

acrylic-template.pdf

Install CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify experimentation and education on low-cost microcontrollers. It makes it easier than ever to get prototyping by requiring no upfront desktop software downloads. Simply copy and edit files on the CIRCUITPY drive to iterate.

CircuitPython Quickstart

Follow this step-by-step to quickly get CircuitPython running on your board.

Download the latest version of CircuitPython for this board via circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.

Save it wherever is convenient for you.

file_8

save_9

To enter the bootloader, hold down the BOOT/BOOTSEL button (highlighted in red above), and while continuing to hold it (don't let go!), press and release the reset button (highlighted in blue above). Continue to hold the BOOT/BOOTSEL button until the RPI-RP2 drive appears!

If the drive does not appear, release all the buttons, and then repeat the process above.

You can also start with your board unplugged from USB, press and hold the BOOTSEL button (highlighted in red above), continue to hold it while plugging it into USB, and wait for the drive to appear before releasing the button.

A lot of people end up using charge-only USB cables and it is very frustrating! Make sure you have a USB cable you know is good for data sync.

You will see a new disk drive appear called RPI-RP2.

Drag the adafruit_circuitpython_etc.uf2 file to RPI-RP2.

drive_10

drive_11

The RPI-RP2 drive will disappear and a new disk drive called CIRCUITPY will appear.

That's it, you're done! :)

circuitpy_12

Safe Mode

You want to edit your code.py or modify the files on your CIRCUITPY drive but find that you can't. Perhaps your board has gotten into a state where CIRCUITPY is read-only. You may have turned off the CIRCUITPY drive altogether. Whatever the reason, safe mode can help.

Safe mode in CircuitPython does not run any user code on startup and disables auto-reload. This means a few things. First, safe mode bypasses any code in boot.py (where you can set CIRCUITPY read-only or turn it off completely). Second, it does not run the code in code.py. And finally, it does not automatically soft-reload when data is written to the CIRCUITPY drive.

Therefore, whatever you may have done to put your board in a non-interactive state, safe mode gives you the opportunity to correct it without losing all of the data on the CIRCUITPY drive.

Entering Safe Mode

This documentation explains entering safe mode on CircuitPython 6.x. The LED behavior will change and reset window will increase in 7.x. This page will be updated accordingly once the change is released.

feather_13

To enter safe mode, plug in your board or hit reset (highlighted in red above). Immediately after the board starts up or resets, it waits 700ms. On some boards, the onboard status LED (highlighted in green above) will turn solid yellow during this time. If you press reset during that 700ms, the board will start up in safe mode. It can be difficult to react to the yellow LED, so you may want to think of it simply as a slow double click of the reset button. (Remember, a fast double click of reset enters the bootloader.)

Once you've entered safe mode successfully, the LED will pulse yellow. If you connect to the serial console, you'll find the following message.

Copy Code
Auto-reload is off.
Running in safe mode! Not running saved code.

CircuitPython is in safe mode because you pressed the reset button during boot. Press again to exit safe mode.

Press any key to enter the REPL. Use CTRL-D to reload.

You can now edit the contents of the CIRCUITPY drive. Remember, your code will not run until you press the reset button, or unplug and plug in your board, to get out of safe mode.

Flash Resetting UF2

If your board ever gets into a really weird state and doesn't even show up as a disk drive when installing CircuitPython, try loading this 'nuke' UF2 which will do a 'deep clean' on your Flash Memory. You will lose all the files on the board, but at least you'll be able to revive it! After loading this UF2, follow the steps above to re-install CircuitPython.

Download flash erasing "nuke" UF2

Code

code_14

Download Project Bundle

Once you've installed the latest version of CircuitPython onto your board, you'll need to grab the code, libraries and any assets included with the project.

Click the download button below to get the code, libraries, and assets all in one!

Download Project Bundle

Copy Code
import time
import os
import board
import displayio
from digitalio import DigitalInOut, Pull
from adafruit_matrixportal.matrix import Matrix
from adafruit_debouncer import Debouncer

SPRITESHEET_FOLDER = "/bmps"
DEFAULT_FRAME_DURATION = 0.1  # 100ms
AUTO_ADVANCE_LOOPS = 3
FRAME_DURATION_OVERRIDES = {
    "three_rings1-sheet.bmp": 0.15,
    "hop1-sheet.bmp": 0.05,
    "firework1-sheet.bmp": 0.03,
}

# --- Display setup ---
matrix = Matrix(bit_depth=4)
sprite_group = displayio.Group(max_size=1)
matrix.display.show(sprite_group)

# --- Button setup ---
pin_down = DigitalInOut(board.BUTTON_DOWN)
pin_down.switch_to_input(pull=Pull.UP)
button_down = Debouncer(pin_down)
pin_up = DigitalInOut(board.BUTTON_UP)
pin_up.switch_to_input(pull=Pull.UP)
button_up = Debouncer(pin_up)

auto_advance = True

file_list = sorted(
    [
        f
        for f in os.listdir(SPRITESHEET_FOLDER)
        if (f.endswith(".bmp") and not f.startswith("."))
    ]
)

if len(file_list) == 0:
    raise RuntimeError("No images found")

current_image = None
current_frame = 0
current_loop = 0
frame_count = 0
frame_duration = DEFAULT_FRAME_DURATION


def load_image():
    """
    Load an image as a sprite
    """
    # pylint: disable=global-statement
    global current_frame, current_loop, frame_count, frame_duration
    while sprite_group:
        sprite_group.pop()

    bitmap = displayio.OnDiskBitmap(
        open(SPRITESHEET_FOLDER + "/" + file_list[current_image], "rb")
    )

    frame_count = int(bitmap.height / matrix.display.height)
    frame_duration = DEFAULT_FRAME_DURATION
    if file_list[current_image] in FRAME_DURATION_OVERRIDES:
        frame_duration = FRAME_DURATION_OVERRIDES[file_list[current_image]]

    sprite = displayio.TileGrid(
        bitmap,
        pixel_shader=displayio.ColorConverter(),
        width=1,
        height=1,
        tile_width=bitmap.width,
        tile_height=matrix.display.height,
    )

    sprite_group.append(sprite)
    current_frame = 0
    current_loop = 0


def advance_image():
    """
    Advance to the next image in the list and loop back at the end
    """
    # pylint: disable=global-statement
    global current_image
    if current_image is not None:
        current_image += 1
    if current_image is None or current_image >= len(file_list):
        current_image = 0
    load_image()


def advance_frame():
    """
    Advance to the next frame and loop back at the end
    """
    # pylint: disable=global-statement
    global current_frame, current_loop
    current_frame = current_frame + 1
    if current_frame >= frame_count:
        current_frame = 0
        current_loop = current_loop + 1
    sprite_group[0][0] = current_frame


advance_image()

while True:
    if auto_advance and current_loop >= AUTO_ADVANCE_LOOPS:
        advance_image()
    button_down.update()
    button_up.update()
    if button_up.fell:
        auto_advance = not auto_advance
    if button_down.fell:
        advance_image()
    advance_frame()
    time.sleep(frame_duration)

View on GitHub

Upload Code, Libraries, and Assets

Unzip the project bundle and upload the files to the CIRCUITPY drive.

Your CIRCUITPY drive should look like this after you've uploaded the code, libraries, and assets.

upload_14

Modify Code

To make the bitmaps display properly on the 32x32 RGB matrix display, look for the following code and update.

You'll also need to update the pins for the Up and Down buttons – These aren't used in this project, but you'll need to update them in order to run the code.

Adjusted Code

Download File

Copy Code
# --- Display setup ---
matrix = Matrix(bit_depth=6, width=32)
sprite_group = displayio.Group(max_size=1)
matrix.display.show(sprite_group)

# --- Button setup ---
pin_down = DigitalInOut(board.D4)
pin_down.switch_to_input(pull=Pull.UP)
button_down = Debouncer(pin_down)
pin_up = DigitalInOut(board.A0)
pin_up.switch_to_input(pull=Pull.UP)
button_up = Debouncer(pin_up)

Sprite Sheets

sheets_15

Animated Sprite Sheets

The sprite sheets are a series of images that are merged together in a single bitmap. Each section in the image is a single frame of the animation that gets played from top to bottom.

It’s really easy to play new animations by just tossing new bitmaps onto the drive. The code automatically cycles through all of the images stored in the bitmaps folder.

Sprite Sheet Bitmap Memes

Download the bitmap images below for your testing. These are pre-made sprite sheets of the infamous party parrot and nyan cat.

cats_16

cats_17

Creating Custom Sprite Sheets

Check out the following guide for lessons on how to create sprite sheet bitmap images.

Guide: Sprite Sheet Animation

Feather Headers

Solder Feather RP2040 Headers

Install a 12-pin and 16-pin strip of male header pins to the Feather RP2040.

Using a breadboard can help keep headers straight while soldering. Solder all of the pins to the RP2040

header_18

header_19

Solder RGB Matrix FeatherWing Headers

Install a 12-pin and 16-pin strip of headers to the RGB Matrix FeatherWing.

Using a breadboard once again to help while soldering.

solder_20

solder_21

Solder DC Jack to RGB Matrix FeatherWing

Install the DC jack onto the RGB Matrix FeatherWing. Solder the DC jack from the bottom side of the PCB. Ensure to use a sufficient amount of solder.

jack_22

jack_23

jack_24

Solder IDC Header to RGB Matrix FeatherWing

Use the notch marking on the silkscreen to determine the correct orientation of the IDC header. Install and insert the IDC header to the top of the PCB. Solder all of the pins.

install_25

install_26

Solder Power Terminal to RGB Matrix FeatherWing

Install and insert the screw-block terminal to the top side of the RGB Matrix FeatherWing. Solder the two pins from the bottom of the PCB.

pins_27

pins_28

Solder Doubler FeatherWing Headers

Use two sets of 12-pin and 16-pin female headers to the Doubler FeatherWing. Start by installing the headers on the top side of the PCB. While holding headers in place, flip the PCB over. Carefully solder all of the pins to the PCB.

place_29

place_30

Assembled Feathers

The Feather RP2040 and RGB Matrix FeatherWing are ready to install on to the Doubler FeatherWing.

Assembled_31

Assembly

Hardware for Doubler FeatherWing

Use the following hardware for securing the Doubler FeatherWing.

  • 4x M2.5 x 4mm screws

  • 4x M2.5 x 6mm screws

  • 4x M2.5 x 6mm FF standoffs

hardware_32

Install Hardware to Doubler FeatherWing

Insert an M2.5 x 4mm screws through one of mounting holes (near the corner) on the Doubler. While holding screw in place, fasten an M2.5 x 6mm FF standoff onto the screw.

Repeat process for a total of four standoffs.

Doubler_33

Doubler_34

Secure FeatherWing Doubler to Frame

Get the Doubler ready to secure onto the frame. Use 4x M2.5 x6mm screws to secure the Doubler to the frame. Place the Doubler over the frame with the standoffs lined up with the mounting holes. Insert and fasten 4x M2.5 x 6mm screws to secure the Doubler to the frame.

Get the Feathers ready to install on the Doubler FeatherWing.

secure_35

secure_36

secure_37

Install Feet

Use the following hardware to secure the feet to the cover.

  • 4x M3 x 6mm screws

  • 4x M3 hex nuts

Insert the M3 hex nuts into the recesses in the inside cover. Firmly press the nuts to install them.

Insert the M3 screws through the holes in the feet. Place the feet over the cover and line up the mounting holes.

Insert and fasten the M3 screws to secure the feet to the cover. Repeat this process for the second foot.

feet_38

feet_39

feet_40

feet_41

Install Acrylic

Place the cut sheet of acrylic into the cover with the matte side facing down, reflective side facing up.

Acrylic_42

Install Grid

Place the grid over the PCB of the 32x32 RGB matrix. Make sure the grid is flush with the PCB and the LEDs are fitted through the squares.

Grid_42

Grid_43

Install Grid to Frame

While holding the grid and PCB together, place the frame over with the Doubler oriented correctly. Press the two together so the frame is fitted over the grid and PCB.

Frame_45

Frame_44

Install Power Cable

Insert the red voltage wire into the positive screw-block on the FeatherWing. Insert the black ground wire into the negative screw-block. Use a screw driver to secure the connectors to the screw-block terminal on the FeatherWing.

Connect the power cable to the power connectors on the back of the RGB matrices PCB.

Cable_46

Cable_47

Install IDC Cable

Connect the IDC cable to the port on the RGB Matrix FeatherWing. Connect the other end of the cable to the HUB75 input on the back of the RGB Matrix.

One of the side clips on the IDC cable may need to be cut in order to fit through the header and DC jack on the RGB Matrix FeatherWing.

Connect_48

Connect_49

Final Assembly

And that’s it! To power the display, plug in the 5V 10A power supply into the DC Jack on the RGB Matrix FeatherWing.

Final_50

complete_51

מק"ט יצרן # 1484
32X32 RGB LED MATRIX PANEL 6MM P
Adafruit Industries LLC
מק"ט יצרן # 4884
ADAFRUIT FEATHER RP2040
Adafruit Industries LLC
מק"ט יצרן # 2890
FEATHERWING DOUBLER - PROTOTYPIN
Adafruit Industries LLC
מק"ט יצרן # 3036
RGB MATRIX FEATHERWING KIT M0 M4
Adafruit Industries LLC
מק"ט יצרן # 4594
BLACK LED DIFFUSION ACRYLIC PANE
Adafruit Industries LLC
מק"ט יצרן # 3299
BLACK NYLON SCREW AND STAND-OFF
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.