Maker.io main logo

Adafruit Optical Fingerprint Sensor

148

2019-08-22 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by Lady Ada

Overview

Secure your project with biometrics - this all-in-one optical fingerprint sensor will make adding fingerprint detection and verification super simple.

Image-1-640-2499

These modules are typically used in safes - there's a high powered DSP chip that does the image rendering, calculation, feature-finding and searching. Connect to any microcontroller or system with TTL serial, and send packets of data to take photos, detect prints, hash and search. You can also enroll new fingers directly - up to 162 finger prints can be stored in the onboard FLASH memory.

 

We like this particular sensor because not only is it easy to use, it also comes with fairly straight-forward Windows software that makes testing the module simple - you can even enroll using the software and see an image of the fingerprint on your computer screen. But, of course, we wouldn't leave you a datasheet and a "good luck!" - we wrote a full Arduino library so that you can get running in under 10 minutes. The library can enroll and search so its perfect for any project. We've also written a detailed tutorial on wiring and use. This is by far the best fingerprint sensor you can get.

  • Supply voltage: 3.6 - 6.0VDC

  • Operating current: 120mA max

  • Peak current: 150mA max

  • Fingerprint imaging time: <1.0 seconds

  • Window area: 14mm x 18mm

  • Signature file: 256 bytes

  • Template file: 512 bytes

  • Storage capacity: 162 templates

  • Safety ratings (1-5 low to high safety)

  • False Acceptance Rate: <0.001% (Security level 3)

  • False Reject Rate: <1.0% (Security level 3)

  • Interface: TTL Serial

  • Baud rate: 9600, 19200, 28800, 38400, 57600 (default is 57600)

  • Working temperature rating: -20C to +50C

  • Working humidy: 40%-85% RH

  • Full Dimensions: 56 x 20 x 21.5mm

  • Exposed Dimensions (when placed in box): 21mm x 21mm x 21mm triangular

  • Weight: 20 grams

Enrolling vs. Searching

There are basically two requirements for using the optical fingerprint sensor. First is you'll need to enroll fingerprints - that means assigning ID #'s to each print so you can query them later. Once you've enrolled all your prints, you can easily 'search' the sensor, asking it to identify which ID (if any) is currently being photographed.

You can enroll using the Windows software (easiest and neat because it shows you the photograph of the print) or with the Arduino sketch (good for when you don't have a Windows machine handy or for on-the-road enrolling).

Enrolling New Users with Windows

The easiest way to enroll a new fingerprint is to use the Windows software. The interface/test software is unfortunately windows-only but you only need to use it once to enroll, to get the fingerprint you want stored in the module.

First up, you'll want to connect the sensor to the computer via a USB-serial converter. The easiest way to do this is to connect it directly to the USB/Serial converter in the Arduino. To do this, you'll need to upload a 'blank sketch' this one works well for "traditional" Arduinos, like the Uno and the Mega:

Copy Code
// this sketch will allow you to bypass the Atmega chip
// and connect the fingerprint sensor directly to the USB/Serial
// chip converter.

// Red connects to +5V
// Black connects to Ground
// White goes to Digital 0
// Green goes to Digital 1

void setup() {}
void loop() {}

The "blank" sketch won't work for "native USB" based Arduinos like the Leonardo, Micro, Zero, etc! Use the Leo_passthru sketch instead!

If you're using a Leonardo, Micro, Yun, Zero, or other native-USB device like ATSAMD21 or ATmega32U4-based controller, use the Leo_passthru sketch instead of the "blank" sketch.

Copy Code
//Leo_passthru
// Allows Leonardo to pass serial data between fingerprint reader and Windows.
//
// Red connects to +5V
// Black connects to Ground
// Green goes to Digital 0
// White goes to Digital 1

void setup() {
  // put your setup code here, to run once:
  Serial1.begin(57600);
  Serial.begin(57600);
}

void loop() {
  
  while (Serial.available())
    Serial1.write(Serial.read());
  while (Serial1.available())
    Serial.write(Serial1.read());
}

Wire up the sensor as described in the sketch comments after uploading the sketch. Since the sensor wires are so thin and short, we stripped the wire a bit and melted some solder on so it made better contact but you may want to solder the wires to header or similar if you're not getting good contact. When you plug in the power, you may see the LED blink to indicate the sensor is working.

If your sensor has all the same-color wires, The first wire from the left is ground, then the two data pins, then power. You'll have to cut, strip and solder the wires.

Image-2-340-48440

RX is the same as the White wire

TX is the same as the Green wire

Image-3-340-49719

If your sensor has different wires, The first wire from the left should be the black wire ground, then the two data pins, RX is the white wire, TX is the green wire then the red power wire. You'll have to cut, strip and solder the wires.

Image-4-640-2500

Start up the SFGDemo software and click Open Device from the bottom left corner. Select the COM port used by the Arduino.

Image-5-640-2501

And press OK when done. You should see the following, with a blue success message and some device statistics in the bottom corner. You can change the baud rate in the bottom left hand corner, as well as the "security level" (how sensitive it is) but we suggest leaving those alone until you have everything running and you want to experiment. They should default to 57600 baud and security level 3 so set them if they're wrong.

If you get an error when you Open Device, check your wiring, try swapping the RX and TX wires on the sensor, that's a common mixup!

Image-6-640-2502

Lets enroll a new finger! Click the Preview checkbox and press the Enroll button next to it (Con Enroll means 'Continuous' enroll, which you may want to do if you have many fingers to enroll). When the box comes up, enter in the ID # you want to use. You can use up to 162 ID numbers.

Image-7-340-2503

The software will ask you to press the finger to the sensor

Image-8-340-2504

You can then see a preview (if you cliecked the preview checkbox) of the fingerprint.

Image-9-640-2505

You will then have to repeat the process, to get a second clean print. Use the same finger!

On success you will get a notice.

Image-10-340-2506

If there's a problem such as a bad print or image, you'll have to do it again.

Searching with the Software

Once you have the finger enrolled, it's a good idea to do a quick test to make sure it can be found in the database. Click on the Search button on the right hand side.

When prompted, press a different/same finger to the sensor.

If it is the same finger, you should get a match with the ID #

Image-11-340-2507

If it is not a finger in the database, you will get a failure notice.

Image-12-340-2508

Wiring for use with Arduino

Once you've tested the sensor, you can now use it within a sketch to verify a fingerprint. We'll need to rewire the sensor. Disconnect the green and white wires and plug the green wire into digital 2 and the white wire to digital 3. (For ESP8266 use 4 & 5, for devices with Hardware UART use 0 & 1)

It is normal for the sensor to blink the LED quickly once powered, after that the LED may stay off until you've started to request data from it

Image-13-340-49718

If your sensor has different wires, The first wire from the left should be the black wire ground, then the two data pins, RX is the white wire, TX is the green wire then the red power wire. You'll have to cut, strip and solder the wires.

Image-14-340-48438

If your sensor has all the same-color wires, The first wire from the left is ground, then the two data pins, then power. You'll have to cut, strip and solder the wires.

RX is the same as the White wire

TX is the same as the Green wire

Arduino UNO & Compatible Wiring

This example sketch uses pins 2 and 3 for software serial (on ATmega328P type boards by default) - Not all boards support Software Serial on all pins so check board documentation! For example on ESP8266 we used 4 & 5

You can power the sensor from 3.3V or 5V

In the diagrams below we show the wires plugged directly into the Arduino. However, this does not work well because the wires are so thin and they dont make contact. You should solder thicker solid core wires to each wire, to make good contact

Image-15-640-2509

Hardware Serial Wiring

If you have a device with hardware serial, you should use that instead. Often this is pins #0 and #1

Image-16-640-48436

Next, you'll need to install the Adafruit Fingerprint sensor library (also available from github).

Open up the Arduino Library Manager:

Image-17-340-48434

Type in Fingerprint until you see the Adafruit Fingerprint library show up!

Image-18-640-48435

Click Install! That's it. Now you should be able to select the File→Examples→Adafruit_Fingerprint→fingerprint example sketch.

Soft & Hard Serial

By default the sketch uses software serial (Arduino UNO & compatibles). If you are using a device with Hardware Serial, e.g does not have a USB-Serial converter chip, use that instead! Usually those are on pins 0 & 1

Copy Code
// On Leonardo/Micro or others with hardware serial, use those! #0 is green wire, #1 is white
// uncomment this line:
#define mySerial Serial1

// For UNO and others without hardware serial, we must use software serial...
// pin #2 is IN from sensor (GREEN wire)
// pin #3 is OUT from arduino  (WHITE wire)
// comment these two lines if using hardware serial
//#include <SoftwareSerial.h>
//SoftwareSerial mySerial(2, 3);

If necessary, uncomment/comment lines for hardware serial support

Upload

Upload it to your Arduino as usual. Open up the serial monitor at 9600 baud and when prompted place your finger against the sensor that was already enrolled.

You should see the following:

Image-19-340-2510

The 'confidence' is a score number (from 0 to 255) that indicates how good of a match the print is, higher is better. Note that if it matches at all, that means the sensor is pretty confident so you don't have to pay attention to the confidence number unless it makes sense for high security applications.

Of course you have to have enrolled a fingerprint first! If you did this using the Windows program, that's good to go. If you have not yet, you should at least have gotten a Found fingerprint sensor! printout. You can go ahead to the next step to enroll fingerprints.

If you get Did not find fingerprint sensor :( check your wiring, maybe swap the RX and TX wire as that's a common issue

If you want to have a more detailed report, change the loop() to run getFingerprintID() instead of getFingerprintIDez() - that will give you a detailed report of exactly what the sensor is detecting at each point of the search process.

Enrolling with Arduino

We did put together a simple sketch for enrolling a new finger via Arduino - its not as easy to use as the Windows program but it does work!

Run the File→Examples→Adafruit_Fingerprint→enroll sketch and upload it to the Arduino, use the same wiring as above.

When you open up the serial monitor, it will ask for you to type in the ID to enroll - use the box up top to type in a number and click Send.

Image-20-340-2511

Then go through the enrollment process as indicated. When it has successfully enrolled a finger, it will print Stored!

Image-21-440-2512

Don't forget to do a search test when you're done enrolling to make sure its all good!

CircuitPython

Image-22-340-49772

If your sensor has different wires, The first wire from the left should be the black wire ground, then the two data pins, RX is the white wire, TX is the green wire then the red power wire. You'll have to cut, strip and solder the wires.

Image-23-340-49773

If your sensor has all the same-color wires, The first wire from the left is ground, then the two data pins, then power. You'll have to cut, strip and solder the wires.

RX is the same as the White wire

TX is the same as the Green wire

Image-24-340-49771

Every CircuitPython board has a hardware UART. Check the product page or look for RX and TX written on the board. Remember that the RX from the sensor goes to the TX on the board! If you have problems try swapping them, its a common mistake

Installing Library

To use the Fingerprint sensor you'll need to install the Adafruit CircuitPython Fingerprint library on your CircuitPython board.

First make sure you are running the latest version of Adafruit CircuitPython for your board.

Next you'll need to install the necessary libraries to use the hardware--carefully follow the steps to find and install these libraries from Adafruit's CircuitPython library bundle. Our introduction guide has a great page on how to install the library bundle for both express and non-express boards.

Remember for non-express boards like the Trinket M0 or Feather M0 Basic, you'll need to manually install the necessary libraries from the bundle:

  • adafruit_fingerprint.mpy

You can also download the adafruit_fingerprint.mpy from its releases page on Github.

Before continuing make sure your board's lib folder or root filesystem has the adafruit_fingerprint.mpy file copied over.

Next connect to the board's serial REPL so you are at the CircuitPython >>> prompt.

Usage

To demonstrate the usage of the sensor, we'll use the example python script included with the library. This sensor is fairly complex so its hard to run it just from the REPL.

Once you've installed the library, run this main.py example on your CircuitPython board.

Copy Code
import time
import board
import busio
from digitalio import DigitalInOut, Direction
import adafruit_fingerprint

led = DigitalInOut(board.D13)
led.direction = Direction.OUTPUT

uart = busio.UART(board.TX, board.RX, baudrate=57600)

# If using with a computer such as Linux/RaspberryPi, Mac, Windows...
#import serial
#uart = serial.Serial("/dev/ttyUSB0", baudrate=57600, timeout=1)

finger = adafruit_fingerprint.Adafruit_Fingerprint(uart)

##################################################


def get_fingerprint():
    """Get a finger print image, template it, and see if it matches!"""
    print("Waiting for image...")
    while finger.get_image() != adafruit_fingerprint.OK:
        pass
    print("Templating...")
    if finger.image_2_tz(1) != adafruit_fingerprint.OK:
        return False
    print("Searching...")
    if finger.finger_fast_search() != adafruit_fingerprint.OK:
        return False
    return True

# pylint: disable=too-many-branches
def get_fingerprint_detail():
    """Get a finger print image, template it, and see if it matches!
    This time, print out each error instead of just returning on failure"""
    print("Getting image...", end="", flush=True)
    i = finger.get_image()
    if i == adafruit_fingerprint.OK:
        print("Image taken")
    else:
        if i == adafruit_fingerprint.NOFINGER:
            print("No finger detected")
        elif i == adafruit_fingerprint.IMAGEFAIL:
            print("Imaging error")
        else:
            print("Other error")
        return False

    print("Templating...", end="", flush=True)
    i = finger.image_2_tz(1)
    if i == adafruit_fingerprint.OK:
        print("Templated")
    else:
        if i == adafruit_fingerprint.IMAGEMESS:
            print("Image too messy")
        elif i == adafruit_fingerprint.FEATUREFAIL:
            print("Could not identify features")
        elif i == adafruit_fingerprint.INVALIDIMAGE:
            print("Image invalid")
        else:
            print("Other error")
        return False

    print("Searching...", end="", flush=True)
    i = finger.finger_fast_search()
    # pylint: disable=no-else-return
    # This block needs to be refactored when it can be tested.
    if i == adafruit_fingerprint.OK:
        print("Found fingerprint!")
        return True
    else:
        if i == adafruit_fingerprint.NOTFOUND:
            print("No match found")
        else:
            print("Other error")
        return False

# pylint: disable=too-many-statements
def enroll_finger(location):
    """Take a 2 finger images and template it, then store in 'location'"""
    for fingerimg in range(1, 3):
        if fingerimg == 1:
            print("Place finger on sensor...", end="", flush=True)
        else:
            print("Place same finger again...", end="", flush=True)

        while True:
            i = finger.get_image()
            if i == adafruit_fingerprint.OK:
                print("Image taken")
                break
            elif i == adafruit_fingerprint.NOFINGER:
                print(".", end="", flush=True)
            elif i == adafruit_fingerprint.IMAGEFAIL:
                print("Imaging error")
                return False
            else:
                print("Other error")
                return False

        print("Templating...", end="", flush=True)
        i = finger.image_2_tz(fingerimg)
        if i == adafruit_fingerprint.OK:
            print("Templated")
        else:
            if i == adafruit_fingerprint.IMAGEMESS:
                print("Image too messy")
            elif i == adafruit_fingerprint.FEATUREFAIL:
                print("Could not identify features")
            elif i == adafruit_fingerprint.INVALIDIMAGE:
                print("Image invalid")
            else:
                print("Other error")
            return False

        if fingerimg == 1:
            print("Remove finger")
            time.sleep(1)
            while i != adafruit_fingerprint.NOFINGER:
                i = finger.get_image()

    print("Creating model...", end="", flush=True)
    i = finger.create_model()
    if i == adafruit_fingerprint.OK:
        print("Created")
    else:
        if i == adafruit_fingerprint.ENROLLMISMATCH:
            print("Prints did not match")
        else:
            print("Other error")
        return False

    print("Storing model #%d..." % location, end="", flush=True)
    i = finger.store_model(location)
    if i == adafruit_fingerprint.OK:
        print("Stored")
    else:
        if i == adafruit_fingerprint.BADLOCATION:
            print("Bad storage location")
        elif i == adafruit_fingerprint.FLASHERR:
            print("Flash storage error")
        else:
            print("Other error")
        return False

    return True


##################################################

def get_num():
    """Use input() to get a valid number from 1 to 127. Retry till success!"""
    i = 0
    while (i > 127) or (i < 1):
        try:
            i = int(input("Enter ID # from 1-127: "))
        except ValueError:
            pass
    return i


while True:
    print("----------------")
    if finger.read_templates() != adafruit_fingerprint.OK:
        raise RuntimeError('Failed to read templates')
    print("Fingerprint templates:", finger.templates)
    print("e) enroll print")
    print("f) find print")
    print("d) delete print")
    print("----------------")
    c = input("> ")

    if c == 'e':
        enroll_finger(get_num())
    if c == 'f':
        if get_fingerprint():
            print("Detected #", finger.finger_id, "with confidence", finger.confidence)
        else:
            print("Finger not found")
    if c == 'd':
        if finger.delete_model(get_num()) == adafruit_fingerprint.OK:
            print("Deleted!")
        else:
            print("Failed to delete")

It's fairly long but it will help you set-up and test your sensor!

When you first start up, you should get something like this:

Image-25-Pt2

If you get an error like RuntimeError: Failed to read data from sensor it means something went wrong - check your wiring and baud rate!

This menu system is fairly simple, you have three things you can do

  • Enroll print - you will use your finger to take images and 'store' the model in the sensor

  • Find print - determine whether a fingerprint is known and stored

  • Delete print - clear out a model

Enrolling Prints

Enrolling a finger print is easy. Type e to start the process. You'll need to select a location. The sensor can store up to 127 print locations. Pick a valid number, then place your finger twice to enroll.

Image-26-540-49767

Note that after success, the Fingerprint templates: [...] printout will include the new template id.

If an error occurs, the sensor will give you an error, such as if the two prints don't match, or if it failed to store or generate a model:

Image-27-540-49768

Finding Prints

Once you've enrolled fingerprints you can then test them. Run the find command, and try various fingers! Once the fingerprint id identified it will tell you the location number, in this case #5

Image-28-540-49769

Deleting Fingerprints

If you made a mistake you can remove fingerprint models from the database. For example, here's how to delete #5. Note the Fingerprint templates: [...] printout changes!

Image-29-540-49774

Downloads

מק"ט יצרן # 153
JUMPER WIRE M TO M VARIOUS
Adafruit Industries LLC
מק"ט יצרן # A000073
ARDUINO UNO SMD R3 ATMEGA328
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.