Maker.io main logo

Bluetooth-Controlled Matrix LED Sign using Bluefruit Connect

226

2024-10-04 | By Adafruit Industries

License: See Original Project Addressable LEDs Displays LCD / TFT

Courtesy of Adafruit

Guide by Trevor Beaton

Overview

adafruit_products_ezgif_com_optimize_15

Express yourself with this Bluetooth-controlled sign using Adafruit's ‎RGB LED Matrix Display, Adafruit nRF52840 Feather running ‎CircuitPython, and the RGB Matrix nRF52840 FeatherWing.

With this project, you can effortlessly display text on the Matrix panel ‎and change the text color with ease through the Bluefruit Connect ‎app. You can display scrolling text on the Matrix display and easily ‎change the color of the text using the Bluefruit Connect app.‎

This setup was initially written for the 64x32 Matrix, but has also ‎been tested on the 64x64 Matrix, 16x32 Matrix, and 32x32 Matrix as ‎well.

setup_1

To complete this project, it is necessary to perform soldering.‎

Parts

CircuitPython for Feather nRF52840

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

The following instructions will show you how to install CircuitPython. ‎If you've already installed CircuitPython but are looking to update it ‎or reinstall it, the same steps work for that as well!‎

Set up CircuitPython Quick Start!‎

Follow this quick step-by-step for super-fast Python power :)‎

Download the latest version of CircuitPython for this board via ‎CircuitPython.org

Click the link above to download the latest UF2 file.‎‎ ‎

Download and save it to your desktop (or wherever is handy).‎

download_2

Plug your Feather nRF52840 into your computer using a known-‎good USB cable.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! So, make sure you have a USB cable you know is good ‎for data sync.

Double-click the Reset button next to the USB connector on your ‎board, and you will see the NeoPixel RGB LED turn green (identified ‎by the arrow in the image). If it turns red, check the USB cable, try ‎another USB port, etc. Note: The little red LED next to the USB ‎connector will pulse red. That's ok!‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

board_3

You will see a new disk drive appear called FTHR840BOOT.‎‎ ‎‎ ‎‎

‎Drag the adafruit_circuitpython_etc.uf2 file to FTHR840BOOT.‎

boot_4

boot_5

The LED will flash. Then, the FTHR840BOOT drive will disappear, ‎and a new disk drive called CIRCUITPY will appear.‎‎

‎That's it, you're done! :)‎

boot_6

Update Bootloader

Your board's bootloader must be 0.6.1 or later to be able to load ‎CircuitPython 8.2.0 or later.‎

Older versions of Adafruit's nRF52840 boards were shipped with a ‎bootloader that does not handle large UF2's, including CircuitPython ‎‎8.2.0 and later, and has other issues. To check whether you need to ‎update the bootloader, double-click the reset button, and look in ‎the ...BOOT drive for INFO_UF2.TXT.‎

Inside that file, check the version number of the bootloader. There ‎are multiple version numbers. Look for the number just after "UF2 ‎Bootloader" on the first line. See the picture below It should be 0.6.1 ‎or newer.‎

inside_7

The dafruit nRF52 Bootloader can be upgraded/downgraded without ‎any additional hardware. There are 3 different ways to update ‎bootloader, each has its pros and cons:‎

  • Use UF2: This is the fastest and safest way to update ‎bootloader. However, it requires your existing bootloader ‎version is at least 0.4.0 and only work with nRF52840 (not ‎nRF52832)

  • Use Arduino IDE: work with all Adafruit nRF52 boards and ‎bootloader version, typo free but may not be the latest ‎bootloader version due to the BSP release cycle

  • Use Command Line: work with all boards and bootloader ‎version (including 3rd party one). This command line uses the ‎back end of the Arduino IDE method above. ‎

Use UF2‎

This is the fastest and safest way to update bootloader. However, it ‎requires your existing bootloader is at least 0.4.0 and only work with ‎nRF52840 (not nRF52832) since UF2 make use of USB MSC interface.‎

Download update-bootloader UF2‎

You need a .uf2 file containing the latest version of the bootloader. ‎The most common updaters are linked below. For updaters for other ‎boards, look for the .uf2 files here that begin with update-...‎

Note if you click the link above, you must scroll down to the UF2 files ‎that begin with the word update as the zip files do not include UF2s. ‎Most users will click the appropriate green button below to select ‎the file for their board.‎

Feather nRF52840 Express bootloader updater UF2 (version 0.8.2)‎

Circuit Playground Bluefruit bootloader updater UF2 (version 0.8.2)

‎ItsyBitsy nRF52840 bootloader updater UF2 (version 0.8.2)‎

CLUE nRF52840 bootloader updater UF2 (version 0.8.2)‎

Feather Sense nRF52840 bootloader updater UF2 (version 0.8.2)‎

Enter Bootloader Mode

Double-click the Reset button on your board, and you will see the ‎NeoPixel RGB LED turn green (identified by the arrow in the image). ‎If it turns red, check the USB cable, try another USB port, etc.‎

Note: on nRF52840 USB Key with TinyUF2 (PID 5199) you need to ‎hold its button while plugging into your PC.‎

Drag & Drop UF2‎

You will see a new BOOT disk drive appear e.g., FTHR840BOOT. ‎Drag the downloaded .uf2 file to FTHR840BOOT. The LED will flash. ‎Then, the FTHR840BOOT drive will disappear. That's it, you have ‎successfully updated your board to the latest version. ‎

drive_8‎ ‎

Issues

If you download the wrong UF2 file for your board, dragging the file ‎to the ...BOOT drive will close the drive but will not update the ‎firmware (as it is the firmware for the wrong board). You can check ‎the INFO_UF2.TXT on the board and see if the firmware was ‎updated (likely with the wrong UF2 file it was not). ‎

If you cannot find the correct UF2 check all the files ‎in https://github.com/adafruit/Adafruit_nRF52_Bootloader/releases for the correct UF2 (they all start with the word update-boardname-bootloader-‎version.uf2 so scroll the list down to the files starting with u.‎

Non Adafruit board firmware updates can be found using this ‎method also.‎

Use Arduino IDE

Arduino IDE Burn Bootloader menu option will pick the correct ‎bootloader binary for your selected board and prevent any ‎command typos or other common errors.‎

Close the Serial Monitor before you click "Burn Bootloader". ‎Afterwards, you shouldn't close the Arduino IDE, unplug the board, ‎launch Serial Monitor etc ... to abort the process. There is a high ‎chance it will brick your device! Do this with care and caution.‎

This is an advanced method: if your existing bootloader version is ‎‎0.4.0 or later, you can use the UF2 method, which is faster and safer.‎

If you have not already done so, set up Arduino IDE for nRF52, using ‎the instructions in Arduino Support Setup.‎

Make sure no other program is attached to the serial port on the ‎board, such as Mu, the Serial Monitor in Arduino, or a terminal ‎program. Then, to start, select the correct board you are using ‎under Tools -> Board.‎

menu_9

Then select "Bootloader DFU for Bluefruit nRF52" for Tools-‎‎>Programmer.‎

programmer_10

Double check all of the following: Board, Programmer...‎

Then select Tools->Burn Bootloader to start the upgrade.‎

burn_10a

After receiving the new Bootloader over the serial connection, the ‎old Bootloader will erase itself! The new bootloader will then be ‎flashed. The process typically takes 30-60 seconds to complete. ‎Make sure you see the "Device programmed" in the output log ‎before launching Serial monitor or uploading a new sketch.‎

Copy Code
Upgrading target on /dev/ttyACM0 with DFU package 
/Adafruit_nRF52_Arduino/bootloader/feather_nrf52840_express/feather_nrf52840_express_bootloader-0.6.2_s140_6.1.1.zip. Flow control is disabled, Dual bank, 
Touch 1200
Touched serial port /dev/ttyACM0
Opened serial port /dev/ttyACM0
Starting DFU upgrade of type 3, SoftDevice size: 151016, bootloader size: 
39000, application size: 0
Sending DFU start packet
Sending DFU init packet
Sending firmware file
########################################
########################################
########################################
########################################
########################################
########################################
########################################
########################################
########################################
############
Activating new firmware

DFU upgrade took 20.50154972076416s
Device programmed.

Drawbacks of this method are that you will need to install the ‎Arduino IDE, and the bundled bootloader may not be the latest one. ‎Check out the next page for a more advanced command line version.‎

Use Command Line

This is an advanced method, which is only necessary if your ‎bootloader is older than 0.4.0. If your existing bootloader version is ‎‎0.4.0 or later, you can use the UF2 method, which is faster and safer.‎

Download Bootloader Package

To update the bootloader, you need a .zip file containing the latest ‎version of the bootloader. The most common bootloader .zip files are ‎linked below. For .zip files for other boards, look for the .zip files ‎here that begin with the name of the board you want to update.‎

Pick the download below for the board that you have. If you have a ‎different board, look for the right .zip file for the board you have at ‎the link just above.‎

Bootloader .zip package for Adafruit Feather nRF52840 (latest ‎version)‎

Bootloader .zip package for Adafruit Feather nRF52840 Sense (latest ‎version)‎

Bootloader .zip package for Adafruit CLUE (latest version)

‎Bootloader .zip package for Circuit Playground Bluefruit (latest ‎version)

Bootloader .zip package for Adafruit ItsyBitsy nRF52840 (latest ‎version)‎

Do not unzip this .zip file after downloading. It will be used as is.‎

Download adafruit-nrfutil

You will also need the utility program adafruit-nrfutil, which has ‎slightly different names on different platforms.‎

adafruit-nrfutil for Linux

On Linux, you can download and install adafruit-nrfutil by doing:‎

Copy Code
pip3 install --user adafruit-nrfutil

adafruit-nrfutil for macOS

On macOS, if you have python3 and pip3 installed, you can install ‎via pip3, as above for Linux. Otherwise download the zip ‎file adafruit-nrfutil-macos...zip from the link below, and then extract ‎the file adafruit-nrfutil from the zip file.‎

adafruit-nrfutil-macos for MacOS (in .zip file)‎

Then make adafruit-nrfutil executable by doing:‎

Copy Code
chmod +x adafruit-nrfutil

adafruit-nrfutil for Windows

Download the .zip file from this link and extract the file adafruit-‎nrfutil.exe.‎

adafruit-nrfutil.exe for Windows (in .zip file)‎

Update Bootloader

To update the bootloader, first connect the board, and then double-‎click the RESET button to get the ...BOOT drive to appear.‎

Different boards will have different boot folder names, but they ‎should all end with BOOT.‎

Updating on Linux

Run a command similar to the one below in a shell ‎window. Substitute the name of the .zip file you downloaded ‎above for the file given below.‎

Copy Code
adafruit-nrfutil --verbose dfu serial --package feather_nrf52840_express_bootloader-0.8.0_s140_6.1.1.zip -p /dev/ttyACM0 -b 115200 --singlebank --touch 1200

Updating on macOS

Find out the device name for the connected board, by doing:‎

Copy Code
ls /dev/cu.*

The device name will be something like /dev/cu.usbmodem411. Use this ‎command, substituting the device name you've ‎discovered. Substitute the name of the .zip file you downloaded ‎above for the file given below. and the name of the .zip package ‎you downloaded above. If you are running it other than where you ‎downloaded adafruit-nrfutil-macos, change the path to the ‎command accordingly. If you installed it via pip3, it's just ‎called adafruit-nrfutil, and it should be in your PATH.‎

Copy Code
./adafruit-nrfutil-macos --verbose dfu serial --package feather_nrf52840_express_bootloader-0.8.0_s140_6.1.1.zip -p /dev/cu.usbmodem411 -b 115200 --singlebank --touch 1200

Updating on Windows

Use this command in the folder where you downloaded the other ‎two files above. You'll need to specify the correct COM port, instead ‎of COMxx. Look in Device Manager->Ports for the name of the COM ‎port (it will be listed as a "USB Serial Device" on Windows 10) after ‎you have double-clicked the RESET button. Substitute the name of ‎the .zip file you downloaded above for the file given below.

Copy Code
adafruit-nrfutil.exe --verbose dfu serial --package feather_nrf52840_express_bootloader-0.8.0_s140_6.1.1.zip --port COMxx -b 115200 --singlebank --touch 1200

Output when Updating

When you run the adafruit-nrfutil program, you will see output ‎similar to this (it will vary slightly depending on your OS).‎

Copy Code
Upgrading target on COM29 with DFU package C:\Users\halbe\Desktop\update-feather-nrf52840-bootloader-0.8.0-windows\feather_nrf52840_express_bootloader-0.8.0_s140_6.1.1.zip. Flow control is disabled, Single bank, Touch 1200
Touched serial port COM29
Opened serial port COM29
Starting DFU upgrade of type 3, SoftDevice size: 151016, bootloader size: 39000, application size: 0
Sending DFU start packet
Sending DFU init packet
Sending firmware file
########################################
########################################
########################################
########################################
########################################
########################################
########################################
########################################
########################################
############
Activating new firmware

DFU upgrade took 21.119003295898438s
Device programmed.

Once done, click the RESET button again - the bootloader will be ‎running!‎

Assembly

assembly_10

Assembling your Bluetooth sign with the RGB LED Matrix Panel is ‎straightforward but will require some soldering.‎

In addition to your Adafruit RGB Matrix FeatherWing Kit, you'll also ‎need a Header Kit for Feather - 12-pin and 16-pin Socket Header Set.‎

header_11

First, you'll need to solder two socket headers to each side of ‎the RGB Matrix nRF52840 FeatherWing.‎

wing_12

wing_13

Next solder the 2x8 IDC header on to the back of the feather.‎

solder_14

Finally, you'll need to solder the 5.08mm terminal block and ‎the 2.1mm DC jack to the feather.‎

solder_15

solder15a

Attach the jumper wires included in the Matrix Panel kit to the ‎terminal block on your Feather board. Remember, the negative sign ‎denotes ground (black wire), while the positive sign is for the 5 volts ‎‎(red wire).‎

attach_16

attach_17

Stack your Adafruit nRF52840 Feather Express onto your RGB Matrix ‎nRF52840 FeatherWing to match the photo above. ‎

stack_18

Next, connect your RGB Matrix nRF52840 FeatherWing to your ‎Matrix panel. Be sure to place your FeatherWing on the LiPo battery ‎socket on the left side. For the correct orientation, the arrows on the ‎Matrix panel should point to your right and upward.‎

Finally, connect your 5V 2A (2000mA) switching power supply to ‎your RGB Matrix nRF52840 Feather Wing's 2.1mm DC jack.

Great! Now, now to get the Bluefruit Connect app.‎

Bluefruit Connect App

flowerstar_19

Use Bluefruit Connect to display text to our Matrix Panel via ‎Bluetooth.‎

The Bluefruit Connect app allows you to wirelessly connect your iOS ‎or Android device to Adafruit Bluefruit LE modules for control & ‎communication with your projects. First, we'll need to download it.‎

Installation and Setup

setup_20

The Bluefruit LE Connect app provides iOS & Android devices with a ‎variety of tools to communicate with Bluefruit LE devices. These ‎tools cover basic communication and info reporting as well as more ‎project specific uses such as Arduino Pin Control and a Color Picker.‎

The iOS app is a free download from Apple's App Store. It requires ‎iOS 11.3 or later and works on iPhones, iPads, and iPod Touches.‎

The Android app is a free download from the Google Play Store. It ‎requires Android 4.4 or later.‎

The app is compatible with these BLE devices from Adafruit, and ‎possibly more:‎

First off - install the app from one of the App stores listed above if ‎you haven't already.‎

Enable Bluetooth

If Bluetooth is disabled on your device, enable it by going ‎to Settings->Bluetooth on your iOS device, or the analogous setting ‎on your Android device.‎

bluetooth_20

Enable Location Services

If you plan to use the app to send location/GPS data to Bluefruit LE, ‎enable Location Services. Enable it on iOS using Settings->Privacy-‎‎>Location Services.‎

location_21

Scan for Devices

On launch, the app will automatically begin to scan for ‎nearby Bluetooth LE devices. Devices are presented in a table ‎view in the order in which they were discovered.‎

Don't forget to turn on Bluetooth on your device! Airplane Mode ‎turns off BLE.‎

iPhone

The following images depict the app when used on the iPhone. The ‎Android app looks similar.‎

iphone_22

The device list will display all BLE devices discovered by the app (not ‎just Bluefruit hardware) - so you may see a quite a few "" or ‎‎<Unknown> entries for devices that don't advertise their name, as ‎seen above.‎

  • To refresh the list and start a new scan, simply swipe down on ‎the current list

  • Each device's signal strength is displayed in the left side of its ‎row

If you tap on the device entry (not on Connect), you'll see more detail ‎about a particular device:‎

device_23

iPad

The following images depict the app when used on the iPad.‎

ipad_24

Tap the middle of a device's table row to reveal its relevant ‎advertisement data.‎

  • Any device listed with a "Connect" button at the right can be ‎accessed in Info mode

  • Any device listed as "UART Capable" can be used with all ‎modes - Info, UART, Pin I/O, & Controller

To use the Bluefruit Connect app with your device it must be "UART ‎capable"! All Adafruit BLE devices implement the UART interface, ‎but other devices may not.

Multiple UART Mode

mode_25

The Multiple UART feature allows to monitor incoming data from and ‎send data to multiple devices simultaneously.‎

To use it:‎

  • Activate the Multiple UART Mode switch

  • Tap Connect next to each device you'd like to include

  • Tap the Start button below the Multiple UART mode to begin.‎

Once connected, you can choose UART or Plotter module to view ‎incoming data from all connected peripherals. In the UART module, ‎you can send data to one or all connected devices at once.‎

Connect

Tap the Connect button on the UART capable list entry you wish to ‎use and choose a connection mode from the menu that appears.‎

connect_26

Troubleshooting

trouble_27

If you’re having trouble finding your Bluefruit device in the scannedperipherals list, ensure the board is powered and not paired with ‎any other BLE devices. If the problem persists, it could be due ‎to caching issues in the iOS or Android operating system. For a fix, ‎try the following:‎

  • Cycle Bluetooth - Turn your mobile device’s Bluetooth radio off ‎and on again in the Settings app

  • Relaunch App - Quit the Bluetooth LE Connect app and restart ‎it. (instructions for iOS & Android)‎

  • Cycle Power - Restart your mobile device by powering it off ‎and restarting.‎

Doing one or both of the above solves most peripheral scanning ‎issues. If you're still having trouble, try searching the Adafruit ‎Support forum for your issue.‎

Code the Matrix Sign

Once you've finished setting up your Adafruit nRF52840 Feather ‎with CircuitPython, you can access the code and necessary libraries ‎by downloading the Project Bundle.‎

To do this, click the Download Project Bundle button in the window ‎below. It will download all needed files as a zipped folder.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2023 Trevor Beaton for Adafruit Industries
# SPDX-License-Identifier: MIT


import time
import board
import displayio
import framebufferio
import rgbmatrix
import terminalio
from adafruit_display_text import label
from adafruit_ble import BLERadio
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.nordic import UARTService

SEND_RATE = 10  # how often in seconds to send text

count = 0

SCROLL_DELAY = 0.05  # delay between scrolls, in seconds

ble = BLERadio()
uart_server = UARTService()
advertisement = ProvideServicesAdvertisement(uart_server)

# Release any previously allocated displays
displayio.release_displays()

matrix = rgbmatrix.RGBMatrix(
    width=64, height=32, bit_depth=1,
    rgb_pins=[board.D6, board.A5, board.A1, board.A0, board.A4, board.D11],
    addr_pins=[board.D10, board.D5, board.D13, board.D9],
    clock_pin=board.D12, latch_pin=board.RX, output_enable_pin=board.TX,
)
display = framebufferio.FramebufferDisplay(matrix, auto_refresh=True)

main_group = displayio.Group()

def scroll(line):
    line.x -= 1
    line_width = line.bounding_box[2]
    if line.x < -line_width:
        line.x = display.width

def update_display(text, color=0xFFFFFF):
    """Update the display with the provided text and color."""
    if len(main_group) > 0:
        main_group.pop()
    text_area = label.Label(terminalio.FONT, text=text, color=color)
    text_area.x = display.width
    text_area.y = 13
    main_group.append(text_area)
    display.root_group = main_group

while True:
    print("WAITING...")
    update_display("WAITING...")
    ble.start_advertising(advertisement)

    while not ble.connected:
        scroll(main_group[0])
        display.refresh(minimum_frames_per_second=0)
        time.sleep(SCROLL_DELAY)

    # Connected
    ble.stop_advertising()
    print("CONNECTED")
    update_display("CONNECTED")

    # Loop and read packets
    last_send = time.monotonic()
    while ble.connected:
        if uart_server.in_waiting:
            raw_bytes = uart_server.read(uart_server.in_waiting)
            received_text = raw_bytes.decode().strip()
            print("RX:", received_text)
            update_display(received_text, color=0x26B7FF)

        if time.monotonic() - last_send > SEND_RATE:
            transmit_text = "COUNT = {}".format(count)
            print("TX:", transmit_text)
            uart_server.write((transmit_text + "\r\n").encode())
            count += 1
            last_send = time.monotonic()

        scroll(main_group[0])
        display.refresh(minimum_frames_per_second=0)
        time.sleep(SCROLL_DELAY)

    print("DISCONNECTED")

View on GitHub

Text Editor

Adafruit recommends using the Mu editor for editing your ‎CircuitPython code. You can get more info in this guide.‎

Alternatively, you can use any text editor that saves simple text files.‎

Upload the Code and Libraries to ‎the Adafruit nRF52840 Feather

After downloading the Project Bundle, plug your Adafruit nRF52840 ‎Express into the computer's USB port. You should see a new flash ‎drive in the computer's File Explorer or Finder (depending on your ‎operating system) called CIRCUITPY. Unzip the folder and copy the ‎following items to the Adafruit nRF52840 ‎Express's CIRCUITPY drive. ‎

  • lib folder

  • code.py

Your Adafruit nRF52840 Express CIRCUITPY drive should look like ‎this after copying the lib folders and the code.py file.‎

files_28

code.py Review

Initialization and Configuration

Download File

Copy Code
SEND_RATE = 10  
count = 0
SCROLL_DELAY = 0.05
ble = BLERadio()
uart_server = UARTService()
advertisement = ProvideServicesAdvertisement(uart_server)
  • END_RATE: Sets how frequently the program sends text over ‎Bluetooth (every 10 seconds)

  • count: A variable initialized to 0, likely used for counting ‎something (such as messages sent)

  • SCROLL_DELAY: Time delay between each scroll movement on ‎the display, set to 0.05 seconds

  • Bluetooth Setup: Initializes a BLE (Bluetooth Low Energy) ‎radio, a UART service for Bluetooth communication, and an ‎advertisement for that service

Display Setup

Download File

Copy Code
displayio.release_displays()

matrix = rgbmatrix.RGBMatrix(
    width=64, height=32, bit_depth=1,
    rgb_pins=[board.D6, board.A5, board.A1, board.A0, board.A4, board.D11],
    addr_pins=[board.D10, board.D5, board.D13, board.D9],
    clock_pin=board.D12, latch_pin=board.RX, output_enable_pin=board.TX,
)
display = framebufferio.FramebufferDisplay(matrix, auto_refresh=True)

main_group = displayio.Group()
  • Display Release: Releases any previously allocated displays to ‎avoid conflicts

  • Matrix Initialization: Sets up the RGB matrix display with ‎specific configurations (size, pins, etc.)

  • Display Initialization: Creates a framebuffer display from the ‎RGB matrix

  • Display Group: Initializes a Group object, a container for display ‎elements‎

Function Definitions

Download File

Copy Code
def scroll(line):
    line.x -= 1
    line_width = line.bounding_box[2]
    if line.x < -line_width:
        line.x = display.width

def update_display(text, color=0xFFFFFF):
    if len(main_group) > 0:
        main_group.pop()
    text_area = label.Label(terminalio.FONT, text=text, color=color)
    text_area.x = display.width
    text_area.y = 13
    main_group.append(text_area)
    display.root_group = main_group
  • scroll() Function: Defines how to scroll text across the display. ‎It moves the text to the left and wraps around it when it ‎reaches the edge

  • update_display() Function: Updates the display with new text. It ‎removes the old text (if any) and adds new text to the display ‎group.‎

The Main Loop

Download File

Copy Code
while True:
    print("WAITING...")
    update_display("WAITING...")
    ble.start_advertising(advertisement)

    while not ble.connected:
        scroll(main_group[0])
        display.refresh(minimum_frames_per_second=0)
        time.sleep(SCROLL_DELAY)

    # Connected
    ble.stop_advertising()
    print("CONNECTED")
    update_display("CONNECTED")

    # Loop and read packets
    last_send = time.monotonic()
    while ble.connected:
        if uart_server.in_waiting:
            raw_bytes = uart_server.read(uart_server.in_waiting)
            received_text = raw_bytes.decode().strip()
            print("RX:", received_text)
            update_display(received_text, color=0x26B7FF)

        if time.monotonic() - last_send > SEND_RATE:
            transmit_text = "COUNT = {}".format(count)
            print("TX:", transmit_text)
            uart_server.write((transmit_text + "\r\n").encode())
            count += 1
            last_send = time.monotonic()

        scroll(main_group[0])
        display.refresh(minimum_frames_per_second=0)
        time.sleep(SCROLL_DELAY)

    print("DISCONNECTED")
  • Outer While Loop: The main loop that runs forever

  • Waiting for Connection: The display shows "WAITING..." and ‎starts advertising for a Bluetooth connection

  • Scrolling Text: Continuously scrolls text on the display while ‎not connected

  • BLE Connection Established: Stops advertising once ‎connected and updates the display

  • Inner While Loop: While connected, it reads data from the ‎UART service, displays it, and sends back a count message at ‎regular intervals defined by SEND_RATE

  • Scrolling and Refreshing Display: Continuously updates the ‎display while connected

  • Disconnect Handling: Prints "DISCONNECTED" to the console ‎when the connection is lost

Usage

adafruit_products_ezgif_com_optimize_16

It's time to display text on the Matrix panel with the code uploaded ‎to your Adafruit nRF52840. Start by opening the Bluefruit Connect ‎app if you don't already have it open.‎

display_29

From there, select the UART terminal module in the features list. ‎Once in the UART terminal, you can just add whatever text you want ‎to display.‎

select_30

Get creative!

מק"ט יצרן # 5362
64X64 RGB LED MATRIX PANEL - 2MM
Adafruit Industries LLC
מק"ט יצרן # 420
ADDRESS LED MATRIX RED/GRN/BLU
Adafruit Industries LLC
מק"ט יצרן # 607
ADDRESS LED MATRIX RED/GRN/BLU
Adafruit Industries LLC
מק"ט יצרן # 4702
ADAFRUIT RGB MATRIX FEATHERWING
Adafruit Industries LLC
מק"ט יצרן # 2278
64X32 RGB LED MATRIX - 4MM PITCH
Adafruit Industries LLC
מק"ט יצרן # 2886
FEATHER HEADER KIT FML
Adafruit Industries LLC
מק"ט יצרן # 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
מק"ט יצרן # 2487
MOD FLORA WEARABLE BLUEFRUIT LE
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.