Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
VHB-Slide17

Shown here is essentially a recap of the features and benefits discussed so far. One additional point not discussed thus far is that 3M VHB Tape allows surfaces made of materials with different thermal expansion coefficients to be bonded by allowing the bond line to slide to accommodate the differential expansion. A more rigid attachment system would create strong tensile and compressive stresses in the two bonded surfaces and potentially result in buckling or cracking.

PTM פורסם ב: