Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
VHB-Slide9

There are three main attributes of 3M VHB Tape that are of interest to electronics applications: bonding, sealing, and shock & vibration absorption. As seen in earlier applications, it is very strong and can seal liquids making it an excellent gasket material for critical applications since it can bond and seal simultaneously. Also, since the foam is a polymer, it has viscoelastic properties and has the capability to absorb and dissipate dynamic loads meaning the foam is tough under shock loading and allows the bond line to withstand high dynamic loads. 

PTM פורסם ב: