Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
BLC-Slide11

The maxiGRIP™ works by applying steady pressure downwards at the center of the heatsink which applies pressure at the most critical point. The long arms of the spring clip allow a range of usable deflection so that packages of different heights can be used in conjunction with a fixed base heatsink. The forces associated with the clip are distributed to the side and underside of the BGA component and are evenly distributed along all four sides.

PTM פורסם ב: