Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
BLC-Slide7

Here is a CFD comparison between maxiFLOW™ and straight fin heatsinks. The result is that maxiFLOW™ also cools, to an extent, other components on the board. Note that the board mounted components numbered 1 through 4 exhibit a 5-6% decrease in temperature relative to the inlet ambient. For this example, the maxiFLOW™ is useful for indirectly cooling smaller critical components.

PTM פורסם ב: