Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Customizable ARM-Based SoC Slide 6

The new SoC FPGA devices are based on a dual-core Arm® Cortex®-A9 processor which is a dual-issue, superscalar processor on the high end of the Arm® processor roadmap. It is designed for high performance, delivering 2.5 MIPS per MHz, and features an integrated floating-point unit and Arm NEON multimedia coprocessor. The dual-core system provides cache coherency between the processors and even extends the coherency to hardware implemented in the FPGA logic.

PTM פורסם ב: