Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
gender
A jack is usually referred to as the female half of the mating connector and the plug is usually referred to as the male half. A standard polarized SMA jack will have a female center contact surrounded by a barrel with external threads. The standard polarized SMA plug will have a male center contact supported by a coupling nut with internal threads. Reverse polarity is a variation which reverses the gender of the center contact, and therefore a reversed polarized SMA jack will have a male center pin and the reversed polarized plug will have a female center contact. Standard polarity SMA connectors are not intermateable with RP-SMA connectors. Depending on the application, a straight or right angle version is available. Right angle versions are ideal for applications with space restrictions.
PTM פורסם ב: