Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
common sma mount
Shown here is a sample image of various ways an RF connector can be mounted to a PCB board. The surface mount and edge mount (also referred to as end-launch) connectors are soldered on the surface of the PCB. Surface mount connectors are soldered to printed circuit boards using a reflow technique. Through hole mounts are inserted through plated holes on the PCB and are soldered using a wave solder technique also.
PTM פורסם ב: