Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
AS5600 Magnetic Position Sensor Slide 4

A pot using the AS5600 is wear-free, robust, and configurable, and can easily be programmed for a custom angular range without using a programmer. The design consists of a board with the AS5600 and mechanics for the sensor magnet, which provides the required mechanical properties as well. This contactless pot offers high reliability and durability and is robust in harsh environments. The angle output is not influenced by any mechanical effects resulting from a contacting wiper.

PTM פורסם ב: