Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Cortex-M3 Introduction and Specific SAM3U Implementation Slide 12
The table shown on this slide highlights the differences between the 144-pin and 100-pin versions of the SAM3U. The 144-pin version offers a 16-bit external bus interface with four chip select lines and an 8-bit multimedia card interface. In addition, both ADCs are upgraded to eight channels in the 144-pin version and one will be able to use up to ninety six GPIOs. The features which are not mentioned in this table are similar in both versions.
PTM פורסם ב: