Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Cortex-M3 Introduction and Specific SAM3U Implementation Slide 16
There are three different SRAM sizes on the different versions of the SAM3U ranging from 32 kB to 8 kB. The 4 kB embedded in the NANDFlash Controller can also be used as an SRAM, which means that the 4 kB are in addition to the embedded SRAM in the product. Lastly, there are 32 bytes that can be used as backup registers in the backup unit.
PTM פורסם ב: