Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 20
The SAM3U is supported by a growing number of development tools such as IAR, Keil and Code Sourcery GNU development tools. Microchip provides software examples for major toolchains: IAR, Keil and GNU. Thanks to the SAM-ICE JTAG interface, the user will be able to program and debug an application in flash or internal RAM. For in-situ Flash programming, the SAM-BA tool can be connected through the USB or serial port. SAM-BA is open source and allows the user to program on-chip or off-chip memories. Developers can customise it to fit with the needs of their application.
PTM פורסם ב: