Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM3U Cortex-M3 Based MCU Introduction Slide 6
The Memory Protection Unit is embedded on the SAM3U. It supports up to eight regions that can be configured from 32 Bytes to 4 GigaBytes. There are different protection rules that are based on the type of transaction, so the different regions can be configured with different access levels. An MPU violation will cause an exception to occur; this is the Memory Management Fault exception. There are several situations when it is useful to use the MPU: to protect data from untrusted user programs, to make memory regions read-only and to isolate memory regions in a multi tasking system.
PTM פורסם ב: