Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
SAM9G46-Pt2-Slide11

The CTR mode uses a set of input blocks called counters to produce a sequence of output blocks that are combined with the plaintext to produce the ciphertext and vice versa. In CTR encryption, the forward cipher function is invoked on each counter block, and the resulting output blocks are exclusive-ORed with the corresponding plaintext blocks to produce the ciphertext blocks. In CTR decryption, the forward cipher function is invoked on each counter block, and the resulting output blocks are exclusive-ORed with the corresponding ciphertext blocks to recover the plaintext blocks.

PTM פורסם ב: