Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
SAM9G46-Pt2-Slide2

DES stands for Data Encryption Standard, which is a famous symmetric-key algorithm previously used in many different applications and is defined in the Federal Information Processing Standards (FIPS) 46-3 document. DES is now considered to be insecure for many applications. This is mainly due to the 56-bit key size being too small. DES ‘Block Size’ which is 64 bits, corresponds to the number of bits in an input or output block of the block cipher.

PTM פורסם ב: