Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
SAMA5D3-Slide5

As shown on this slide, using the Nbench performance benchmarks, the SAMA5D3 has almost double the performance of a device using the Cortex-A8 core with VFPU v3 even though the Cortex device runs faster. Using the Whetstone benchmark, the SAMA5D3 also has double the performance at equivalent processor speeds. Even with the Cortex-A8 device running at 720 MHz, the SAMA5x outperforms it in the Whetstone benchmark. For additional information on the benchmarks, please visit: Nbench-byte at http://en.wikipedia.org/wiki/NBench or Whetstone at http://en.wikipedia.org/wiki/Whetstone_%28benchmark%29.

PTM פורסם ב: