Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Slide3
The MK-R LED is another barrier breaking high power LED from Cree, delivering up to 200 lm/W. This breakthrough is fast on the heels of the 186 lm/W delivered by the recently announced Cree XLamp XM-L2 LED, the industry’s brightest, highest-performing, single die LED. These two recent announcements further establish Cree’s track record for turning R&D breakthroughs into commercially available products in 2-3 years.
PTM פורסם ב: