Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Image of CUI Devices Buzzer Overview - Decibels

A decibel is the scaled logarithm of the ratio of a measured value with respect to a reference value. Decibels are useful because they can show a huge range of values in a small space. For instance a sound pressure scale going from 0 - 120 dB can represent sound pressures from 20 μPa (micro-pascals) to 120,000,000 μPa. This roughly represents the lowest SPL a human can hear all the way up to uncomfortably loud sounds. The generally accepted value for “Pref” in the formula shown here is 20 μPa.

PTM פורסם ב:
PTM Updated on: 2021-10-11