Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Image of CUI Devices Buzzer Overview - Resonant Frequency

Every system has a particular frequency that it tends to vibrate at. For instance, if a string on a guitar is plucked that string will vibrate very near or at its resonant frequency. By driving a system at its resonant frequency, very large displacements relative to the input signal strength can be achieved. Driving a buzzer with an input signal that has the same frequency as the buzzer’s resonant frequency will create the greatest SPL with the least input power.

PTM פורסם ב:
PTM Updated on: 2021-10-11