Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
GaN-Power-Slide10

Now, at an even higher input voltage POL conversion, shown here the engineer can see the efficiency of a converter running at 500Khz with the EPC2105. This 80V half-bridge eGaN IC can convert 48V directly to 1V efficiently. At 16A, peak efficiency is over 80% and is achieved for the full buck converter system. This conversion eliminates two stages that are normally required for this voltage conversion in Datacom systems.

PTM פורסם ב: