Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
GaN-Power-Slide3

For applications requiring a more symmetric device ratio, such as brick power supplies, motor drives, and class D audio, there are also devices with two equal sized dies. Again, the layout features interleaved switch node, input voltage, and power ground leads to enhance inductive cancellation. The high-side FET, Q1, has a gate and a gate return lead to reduce the effects of common source inductance that could slow down the upper device.

PTM פורסם ב: