Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Image of Flexxon X-PHY® M.2 2280 SSD - Operation Flow for Android/IOS

When the user first uses the X-PHY® connect mobile application, they set the email, password and user name. To pair with the X-PHY SSD, click on the Bluetooth button and select the respective X-PHY. If the user would like to review the event log, click on the event button. For unlocking the locked X-PHY SSD, click on the unlock button, enter the SSD password, and then the authenticator OTP and the drive will be unlocked. Power off the X-PHY SSD, then power on again for normal usage.

PTM פורסם ב: