Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
designing with hard3
The FT800 audio output is PWM. The audio is buffered and filtered in order to provide a clean, quality output. A three-stage passive filter is the minimum recommended type. In addition to the audio filtering, a power supply filter is also recommended to remove any unwanted noise from the 18-bit LCD interface. Careful PCB routing and separated grounds are also recommended. The circuit noted above is present on the FT800 evaluation boards and modules.
PTM פורסם ב: