Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
usb-icp-lpc2k interface
Although this version can be used with an SAB, it can also be used to connect directly to the user’s target. This is done through the supplied 18” target cable. All that is required by the user is to incorporate a small 6-pin, 0.1” header on their target as shown in this example. Please note that this is an example only and should not be used for design purposes. Please consult an application datasheet for specific details.
PTM פורסם ב: