Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
bga socket adapter for use FTDI website
If hardware availability is an issue to support a customer’s BGA packaged part, then the SAB may be what is needed. The SAB will allow them to program their device in standalone mode and provides a platform for fine pitch parts in the TFBGA100, 180, and 208 packages. The kit includes an RJ45 Ethernet style cable that interfaces with the USB-ICP device. The SAB also includes a set of onboard LEDs for test purposes. A test program called blink.hex can be downloaded from www.teamfdi.com.
PTM פורסם ב: