Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
DHR-Slide6

The DHR is available in a number of current ranges. The output of the DHR is not designed to drive a heavy load and the next stage’s input impedance should exceed 10 kΩ. The DHR, as an open loop device can withstand significant overloads, up to 30,000A turns. The fundamental accuracy of the DHR at 25°C is 1%. The secondary connection is either a Phoenix connector or Molex Mini-Fit.

PTM פורסם ב: