Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
MAX-Slide6

The block diagram on this slide shows a simplified example of how the MAX1722X products fit into a wearable application. The efficient boost circuit provides the 5V rail necessary to power the optical heart rate device, which requires a higher voltage rail to power the LEDs, while enabling the circuit to run from a low voltage battery, such as a zinc-air. Additional low voltage power rails to the microcontroller are not shown.

PTM פורסם ב: