Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
HowTo-Slide12

Next, press query so the Universal Communicator can identify which controller it is attached to. To load the images onto the Universal Communicator click batch pictures, select the switch type then import the images by pressing the import batch button. A new window will appear, locate the images and click open. Next, click on edit attributes and a new window will appear. This is where any changes can be made to the attribute block before downloading. If no changes are needed, click download batch attributes. Once the download is complete click ok and close the window. The final step to downloading the images is to click on download batch at the bottom of the Universal Communicator window. The Universal Communicator will start downloading the images. Once the download is complete, click yes to close the pop-up window and reset the controller. The IS-DEV Kit-7 will start to display and change images based on what has been programmed into the Development Kit.

PTM פורסם ב: