Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
HowTo-Slide4

Here NKK will describe the following 3 steps for programming the IS-DEV Kit-7 for operation. Step 1 is creating and saving images in a folder. The images can be created in any graphic software such as Paint or Photoshop. The image size must be 64 x 48 pixels and must be saved as 24-bit Bitmap. Additionally, users will want to name the images so the slide or video are in sequential order. Step 2 is loading images into the Universal Communicator and inputting attribute values. The Universal Communicator loads the images from the folder in order by file name. The Universal Communicator will display what address each image will have allowing the user to input attributes which are a set of addresses that tells the controller how to change the images based on switch activity and time. Step 3 is downloading the images and attributes to the Development Kit.

PTM פורסם ב: