Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
MC9RS08KA8-Slide14

This table offers a brief comparison between the devices in the KA8 family. The key specifications to pay attention to are that these devices are available in 16- and 20-pin versions, both SOIC and PDIP packages, and share many of the features between the 16- versus the 20-pin devices. The main thing that is lost when moving from one device to the other is the number of GPIOs.

PTM פורסם ב: