Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
HFR-Slide13

In addition, Omron adopted resin parts on the exterior case and the bottom of the relay. Metal cases that are often found in high frequency relays have the problem that the probe pins short circuit through the metal case during the inspection of the relay mounting board and damage the board and parts, but this product can prevent this issue. At the same time, since pattern wiring can be made right under the bottom of the relay, improvement of freedom of circuit design and loss of signal wiring are reduced.

PTM פורסם ב: