Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
HFR-Slide2

In response to the requirements of high frequency compatibility from the semiconductor tester industry, Omron has developed a differential transmission relay in the 8GHz band within the G6K-RF series. The important features for this market are shown here. It can be used for ATE, various applications using differential transmission methods and other applications requiring higher frequency characteristics.

PTM פורסם ב: